Guangxi Petrochemical Revamps Hydrogen Unit With Honeywell Uop Technology

Honeywell UOP Polybed‚Ñ¢ PSA technology enabled CNPC Guangxi Petrochemical Company to produce high-purity hydrogen.

DES PLAINES, Ill., Aug. 31, 2017 /PRNewswire/ -- Honeywell (NYSE: HON) announced today that CNPC Guangxi Petrochemical Company has successfully converted its existing pressure swing adsorption (PSA) unit to Honeywell UOP Polybed' PSA technology, enabling it to produce high-purity hydrogen.

The newly upgraded unit, located in Qinzhou in China's Guangxi Province, now supplies hydrogen at 99.9 percent purity and with increased hydrogen recovery for Guangxi Petrochemical's hydrotreating units, which use the hydrogen to extract impurities from the feedstock.

"The quality of hydrogen is essential to the operation of any refinery or petrochemical plant because it helps to determine the efficiency of the entire complex," said Rachelle Goebel, vice president and general manager, Gas Processing and Hydrogen at Honeywell UOP. "This revamp of an existing unit shows that customers in China can upgrade to the highest-quality source of hydrogen production without a costly and disruptive unit replacement."

The Honeywell UOP Polybed PSA technology addresses several issues faced by many manufacturers in China, such as low recovery rates and purity, control valve leakage and poor or inconsistent performance.

CNPC Guangxi Petrochemical selected the Honeywell UOP technology due to its experience with another Polybed unit that went into service in 2014. This unit has proven to be a highly reliable source of high-purity hydrogen that is easy to operate.

The PSA process uses proprietary UOP adsorbents to remove impurities at high pressure from hydrogen-containing process streams, allowing hydrogen to be recovered and upgraded to more than 99.9 percent purity to meet refining needs. In addition to recovering and purifying hydrogen from steam reformers and refinery off-gases, the Polybed PSA system can be used to produce hydrogen from other sources such as ethylene off-gas, methanol off-gas and partial-oxidation synthesis gas.

Since the first small, four-bed hydrogen PSA system was commercialized in 1966, Honeywell UOP has significantly improved Polybed PSA systems by incorporating new generations of adsorbents, enhanced cycle configurations, modified process and equipment designs, and more reliable control systems and equipment. To date, Honeywell UOP has installed 1,071 Polybed PSA units in more than 70 countries.

Honeywell UOP's Gas Processing and Hydrogen business offers technology, equipment and materials to treat and process natural gas, as well as to purify hydrogen used in refineries. Its gas technologies extract water, mercury, sulfur, carbon dioxide and other contaminants from raw natural gas, and recover valuable natural gas liquids (NGLs). These solutions are offered as efficient pre-engineered equipment packages or as licensed technology.

Honeywell UOP (www.uop.com) is a leading international supplier and licensor of process technology, catalysts, adsorbents, equipment, and consulting services to the petroleum refining, petrochemical, and gas processing industries. Honeywell UOP is part of Honeywell's Performance Materials and Technologies strategic business group, which also includes Honeywell Process Solutions (www.honeywellprocess.com), a pioneer in automation control, instrumentation and services for the oil and gas, refining, petrochemical, chemical and other industries.

Honeywell (www.honeywell.com/us/en) is a Fortune 100 software-industrial company that delivers industry specific solutions that include aerospace and automotive products and services; control technologies for buildings, homes, and industry; and performance materials globally. Our technologies help everything from aircraft, cars, homes and buildings, manufacturing plants, supply chains, and workers become more connected to make our world smarter, safer, and more sustainable. For more news and information on Honeywell, please visit www.honeywell.com/us/en/news.