Honeywell Implements Advanced Process Control At Bashneft Refineries

Honeywell Profit® Controller and Profit® SensorPro allowed the refineries to significantly increase the output of target products, among other indicators.

 

 

MOSCOW, Dec. 14, 2017 /PRNewswire/ -- Honeywell (NYSE: HON) Process Solutions (HPS) announced its advanced process control (APC) at the Bashneft oil refining complex (part of Rosneft Oil Company) has demonstrated high efficiency, paying for itself in the first year of operation.

 

Honeywell Profit® Controller and Profit® SensorPro allowed the Bashneft refineries to significantly increase the output of target products, decrease energy usage, improve the stability of their quality indicators and the overall plant operational efficiency. The APC software solutions are elements of the innovative Honeywell Profit® Optimization Suite.

"Honeywell products are able to fully perform the work of an operator, automatically controlling a separate unit or an installation as a whole," said Alexei Zenkevich, country business executive, HPS in Russia, Belarus, and Armenia. "Complex automation also reduces the impact on the process of external factors, such as changes in raw material properties, production tasks and inaccurate actions of operators."

Profit Controller is software for multivariable technological process control based on a predictive model. The system contains the optimal set of algorithms for automatic control, using the data of the technological process and virtual analyzers as input signals, and allows users to track the quality of the products and the profitability of production in real time. Profit SensorPro is the auxiliary software that performs the function of virtual analyzers. In real time it calculates the quality indicators based on the measurable parameters (temperature, pressure, raw material consumption, etc.). This enables users to control the quality of products online without waiting, for example, for a manual sampling and laboratory analysis.

Tests and the pilot implementation of the system were conducted beginning in 2013 and were rolled out at several other facilities since that time. Currently, five advanced process control systems are in operation at the Bashneft oil refining complex.

For more information about these Honeywell products, visit Honeywell Profit® Optimization Suite.

Honeywell Process Solutions (www.honeywellprocess.com) is a pioneer in automation control, instrumentation and services for the oil and gas; refining; pulp and paper; industrial power generation; chemicals and petrochemicals; biofuels; life sciences; and metals, minerals and mining industries. It is also a leader in providing software solutions and instrumentation that help manufacturers find value and competitive advantage in through Honeywell Connected Plant, Honeywell's Industrial Internet of Things (IIoT) solution. Process Solutions is part of Honeywell's Performance Materials and Technologies strategic business group, which also includes Honeywell UOP (www.uop.com), a leading international supplier and licensor of process technology, catalysts, adsorbents, equipment, and consulting services to the petroleum refining, petrochemical, and gas processing industries.

Honeywell (www.honeywell.com/us/en) is a Fortune 100 software-industrial company that delivers industry specific solutions that include aerospace and automotive products and services; control technologies for buildings, homes, and industry; and performance materials globally. Our technologies help everything from aircraft, cars, homes and buildings, manufacturing plants, supply chains, and workers become more connected to make our world smarter, safer, and more sustainable. For more news and information on Honeywell, please visit www.honeywell.com/us/en/news.