Fuji Oil Using New Honeywell Uop Catalyst
JULY 30, 2018
Fuji Oil Using New Honeywell UOP Catalyst to Increase Production of Aromatics
Customized cryogenic plant recovers high rates of valuable natural gas liquids from natural gas
DES PLAINES, Ill., July 30, 2018 – Honeywell (NYSE: HON) today announced that Fuji Oil Co., Ltd. has begun using Honeywell UOP’s new R-364 Platforming™ catalyst to produce more aromatics for chemical production at its Sodegaura Refinery on Tokyo Bay in Chiba Prefecture, Japan.
The R-364 catalyst converts naphtha feedstock into aromatics, which are used to make petrochemical compounds, or blended into gasoline to improve its octane rating. The high-activity catalyst features an innovative design that can increase production of a CCR Platforming unit by up to 10 percent.
“We count on UOP to develop new catalysts that improve our economics,” said Daiki Imai, General Manager of Operation Management Department for Fuji Oil. “The R364 catalyst is a drop-in replacement catalyst that effectively increases our capacity and flexibility.”
“Fuji Oil selected the R-364 catalyst because it can increase the refinery’s production of aromatics by boosting throughput of the existing CCR Platforming unit,” said Mike Cleveland, senior business director for Honeywell UOP’s refining catalysts product line. “The catalyst meets Fuji Oil’s requirements for performance, product quality and economics without modifications or investment in new equipment.”
Demand for gasoline in Japan has been declining since reaching a peak in 2004. Japanese refiners such as Fuji Oil have turned to manufacturing higher-value aromatics such as chemical grade benzene and mixed xylenes instead of gasoline. These aromatics have a greater value than motor fuels.
Honeywell UOP introduced the R-364 catalyst in 2017. It retains all the properties of the previous R-264 catalyst, but with better activity and lower coke production, which improves the efficiency of catalytic reactions. As a result, the R-364 catalyst is a drop-in replacement for the R-264 catalyst that increases yields of gasoline, aromatics and hydrogen while producing less coke.
The CCR Platforming process is a continuous catalytic reforming process used throughout the petroleum industry to convert low-quality naphtha into blending stocks for gasoline, aromatics for plastics production and high-purity hydrogen. The CCR Platforming process is in operation at more than 250 customer sites.
Fuji Oil Company, Ltd., imports crude oil and engages in refining, production, processing, storage, export and sale of petroleum products and petrochemical feedstocks. It also distributes petroleum products to clients in Japan by sea, rail, road, and pipeline.
Honeywell UOP (www.uop.com) is a leading international supplier and licensor of process technology, catalysts, adsorbents, equipment, and consulting services to the petroleum refining, petrochemical, and gas processing industries. Honeywell UOP is part of Honeywell’s Performance Materials and Technologies strategic business group, which also includes Honeywell Process Solutions (www.honeywellprocess.com), a pioneer in automation control, instrumentation and services for the oil and gas, refining, petrochemical, chemical and other industries.
Honeywell (www.honeywell.com) is a Fortune 100 diversified technology and manufacturing leader, serving customers worldwide with aerospace products and services; control technologies for buildings, homes, and industry; turbochargers; and performance materials. For more news and information on Honeywell, please visit www.honeywell.com/newsroom.
# # #
Contact:
John Simley
847-391-2278
john.simley@honeywell.com